Post Go back to editing

ESD resistance of ADA4051-2

Thread Summary

The user is experiencing static-related breakdowns with the TLV522DGKR and is evaluating the ADA4051-2 as an alternative. The ADA4051-2 has a Human Body Model (HBM) ESD rating of ±4000V (Class 3A), which is provided in the final answer.
AI Generated Content
Category: Datasheet/Specs
Product Number: ADA4051-2

Hi 

I'm using TLV522DGKR. but the IC broken down by static sometimes.

Then I would like to evaluate other chip. also, I found ADA4051-2 and planning to evaluate the chip.

According to the datasheet, ADA4051-2 has clamp diode and limit the input current to 10 mA. However, it does not mentioned VESD.

if you have VESD information like HBM, I would like to know.

Best regards

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.