Post Go back to editing

ESD resistance of ADA4051-2

Thread Summary

The user is experiencing static-related breakdowns with the TLV522DGKR and is evaluating the ADA4051-2 as an alternative. The ADA4051-2 has a Human Body Model (HBM) ESD rating of ±4000V (Class 3A), which is provided in the final answer.
AI Generated Content
Category: Datasheet/Specs
Product Number: ADA4051-2

Hi 

I'm using TLV522DGKR. but the IC broken down by static sometimes.

Then I would like to evaluate other chip. also, I found ADA4051-2 and planning to evaluate the chip.

According to the datasheet, ADA4051-2 has clamp diode and limit the input current to 10 mA. However, it does not mentioned VESD.

if you have VESD information like HBM, I would like to know.

Best regards

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.