AD8436
Recommended for New Designs
The AD8436 is a new generation, translinear precision, low
power, true rms-to-dc converter loaded with options. It computes a precise dc equivalent of...
Datasheet
AD8436 on Analog.com
I have used this IC AD8436 for my application. I have connected the IC in the dual supply configuration as per given in the data sheet. Now, the problem is that I am not getting output at OUT pin in the IC
My inputs are:
Supply : +15 and -15V
Input signal : 200mV, 26Hz signal
What can be the possible reasons, or there is any pin to turn ON the RMS core part of the IC.
Hi Upreti ,
Good day. Based on the schematic you shared, it seems you have followed the part's typical application and I don't see any issue on that. If it is possible, can you share the waveforms? To check if the RMS core is working, you can use the test circuit from the datasheet:
Also, here is an application circuit as a reference for using the AD8436. Thank you.
Regards,
Gilbeys
Hi Upreti ,
Good day. Based on the schematic you shared, it seems you have followed the part's typical application and I don't see any issue on that. If it is possible, can you share the waveforms? To check if the RMS core is working, you can use the test circuit from the datasheet:
Also, here is an application circuit as a reference for using the AD8436. Thank you.
Regards,
Gilbeys