Post Go back to editing

Circuit made with this IC not working

Thread Summary

The user encountered no output at the OUT pin of the AD8436 in a dual supply configuration with a 200mV, 26Hz input signal. The issue was resolved by following the test circuit from the datasheet and an application note (AN-1341). The user confirmed that using non-polar capacitors for the series and averaging stages did not affect the IC's performance.
AI Generated Content
Category: Hardware
Product Number: AD8436 , AD843

I have used this IC AD8436 for my application. I have connected the IC in the dual supply configuration as per given in the data sheet. Now, the problem is that I am not getting output at OUT pin in the IC

My inputs are:

Supply : +15 and -15V

Input signal : 200mV, 26Hz signal

What can be the possible reasons, or there is any pin to turn ON the RMS core part of the IC.

Parents Reply Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.