I am seeking to create the correct startup sequence for the ADA4870.
The datasheet indicates that for the chip to start, the ON pin (4) must be held low, but that the same pin should be floating during operation to enable short-circuit protection. To me, this seems to imply a tri state logic input. The datasheet does not indicate how long the ON pin should be held low.
I have created a proposed schematic that uses the TC7SZ125F to provide the startup logic. I use a simple RC timer to hold the pin low for a few milliseconds after which I return it to a floating state.
My application requires a DC bias on the output, and that circuitry (R3, R6, and C7) appears here, but isn't relevant to the question.

Can someone comment on whether this is the correct operation.
I have taken the liberty of uploading my PCB layouts as well, as I would love comments. I have chosen a 4-layer stackup with additional 5V and ground planes.
In my application, I do not need to source a lot of power, so I have not been extravagant with thermal planes, though I intend to manufacture the board with the bottom copper plane exposed.


This is similar to a question posed 5 years ago regarding the same chip: ez.analog.com/.../ada4870-on-terminal-transition-time