Post Go back to editing

Increasing current

Thread Summary

The user seeks to increase the current capability of an LT3092-based current sink from 200mA to 350mA while maintaining low noise. The final answer suggests using the LT3088, which can handle higher currents without requiring input or output capacitors for stability. Alternatively, paralleling LT3092s with ballast resistors can achieve higher current, but this method may introduce power dissipation issues. The LT3045 is also recommended for even lower noise.
AI Generated Content
Category: Hardware
Product Number: LT3092

Hi Forum,

We are using the LT3092 in a controlled current sink application, very similar to the diagram "DAC Controlled Current Source" as shown in the Data Sheet Typical Applications.

Our application is in the field of laser and optics, so an extremely low-noise sink is required - hence the use of the LT3092.

However, our next product requires more than 200mA, probably up to about 350mA.

The datasheet does reference two ideas, "Paralleling Current Sources for Higher Current" and "Paralleling LT3092s with Ballast Resistor".

1. We must operate as a current sink, not source. How would these two ideas transfer to the sink topology?

2. Is there an alternate method of utilizing a single LT3092 plus additional cheaper components, to increase the current whilst retaining low noise?

Thanks

David

Thread Notes

  • Hi David,

     

    I will look into your ticket and get back to you as soon as possible.

     

    Kind regards

  • According to the 800mA LT3088 datasheet, "The LT3088 does not require input or output capacitors for stability in many current-source applications."   That means you can just replace the LT3092 in your DAC Controlled Current Source reference design with the LT3088 to get higher current.   I may not completely understand the "Connect Two LT3092s for Higher Current" and "Parallel Devices" reference designs in the LT3092 datasheet you cite.  The ballast resistors may be necessary if you use one reference voltage to control two current sources and you want precise current sharing.  The "Connect Two LT3092s for Higher Current" reference design may ensure stability as well.  Otherwise, you can connect these current sources in parallel just like the ideal ones you studied in engineering school.  Just reference these circuit to VIN to get a current source and reference them to ground to get a current sink.  You can add a resistor from the IN pin to the OUT pin on a LT3092 current source/sink to increase current capability and I would not expect the resistor to increase noise since the output will still be regulated for low noise up to very high frequencies, but there is then a dependance on your circuit's input supply and load voltages for proper operation.  Also, the parallel resistor just dissipates power for some conditions, and most customers don't want that.  Consider the LT3045-type devices for even lower noise.  

  • It would be great if you could add "LT3092" to your post title to make the post a little easier to find.  Thank you.    

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.