Dear ADI Support Team,
I would like to ask about the proper use of the FB (pin 11) of the ADA4870.
Please find attached a simplified schematic showing the intended configuration.
The amplifier is used to drive the gate of an external N-channel MOSFET.
The load current is sensed through a low-side shunt resistor (330 mΩ × 3 in parallel), and the sensed voltage is fed back to the inverting input (INN) through a resistor network.
The non-inverting input receives the control signal.
In this configuration, the feedback loop is closed through the shunt resistor and INN. The FB pin is currently not connected.
My questions are as follows:
-
Is it mandatory to connect a feedback resistor to the FB pin in this type of configuration?
-
If the FB pin is left floating, what issues may occur (for example, loop instability, oscillation, internal bias disturbance, or output stage malfunction)?
-
Is the FB pin internally connected to the compensation network or output stage?
-
If the FB pin is not used, what is the recommended way to terminate it?
The load includes a diode-type device and local decoupling capacitors, as shown in the schematic. The MOSFET gate presents a capacitive load to the amplifier output.
I would appreciate your guidance on the correct handling of the FB pin in this configuration.
Best regards,