Post Go back to editing

AD736 Input Voltage Range

Thread Summary

The user inquired about the AD736's input voltage range and lack of internal protection diodes. The final answer confirmed that the AD736's input voltage (Vin) should not exceed ±Vs and does not include internal protection diodes. External protection, such as a resistor and diode pair, is recommended during power-up to prevent input voltage from exceeding the supply voltage rails.
AI Generated Content
Category: Datasheet/Specs
Product Number: AD736

Hello.

I have a question about AD736.

Regarding the absolute maximum ratings, the input voltage Vin (Pin 2) is specified as ±Vs.
Does this IC not incorporate a protection diode?

Is there a reason it doesn't follow the voltage range specifications seen in other ICs, such as -Vs-0.5 to +Vs+0.5V?

During power-up, each pin rises from GND potential. I'm struggling with how to implement input protection relative to Vin.

Best regards.

  • Hello  

    Thank you for your question regarding the AD736.

    The absolute maximum ratings for the input voltage Vin (Pin 2) of the AD736 are specified as ±Vs, which means the input voltage should not exceed the supply voltage levels. Unlike many other ICs that incorporate internal protection diodes, the AD736 does not have such diodes. This is why the input voltage range is specified as ±Vs rather than the more common -Vs-0.5V to +Vs+0.5V range seen in ICs with internal protection diodes.

    During power-up, when each pin rises from GND potential, it is crucial to implement external protection measures to ensure the input voltage does not exceed the supply voltage rails. You can use a resistor and diode pair for AC line connection measurements, as shown in the datasheet:

    For more detailed information, you can refer to the AD736 datasheet: AD736 (Rev. I)

    Best regards,
    Paul

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.