Post Go back to editing

Problem with the Howland current source design

Thread Summary

The user designed a Howland current source using the LTC6091, which worked in simulation but saturated to the positive supply when a complex load was connected in practice. The issue was caused by DC current due to the offset voltage and the DC resistance of the complex load, leading to instability. Adding a 10uF capacitor in the positive feedback loop resolved the problem.
AI Generated Content
Category: Hardware
Product Number: LTC6091

I designed a howland current source using LTC6091. In simulation, it worked for both resistive and complex load. But practically, it only works for a resistive load or a resistor in parallel with a complex load. After connecting the complex load, the output saturates to positive supply. Does it have a stability problem?

2806.HowlandCurrentPump_SingleOpamp_complexLoad.asc

Thread Notes

Parents Reply Children
  • Hi  ,

    As an initial check, I test and verify that the model matches the datasheet. It appears that the LTspice model has a more stable characteristic compared to the actual data in the datasheet, which is why it seems stable in the simulation. 

    By connecting your complex load to your actual prototype board, does it have any cables in it? Cables do introduce instability in some aspects, then we need to add this to the analysis.

    Also, which part of the circuit is the complex load you are referring to?

  • The offset voltage was causing some DC current at the output. The DC resistance of the complex load is around 8k ohms. The DC voltage across the load was causing positive feedback to increase, resulting in instability. Adding a 10uF capacitor in the positive feedback solved the problem.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.