Post Go back to editing

AD8629 dual opamp giving high offset.

Category: Hardware
Product Number: AD8629

Hey all,

I am working with following circuit using dual op-amps with in AD8629. I am setting 0.1V at input of the first opamp which is acting as a buffer. Here everything is working fine with lower offset of 0.01mV.

Circuit Schematic

The second opamp is maintaining 0.1V across 10K resistor which is setting the 10uA of current. But here with the second opamp if I measure across the resistor R6 there is 0.54mV offset while the input offset of the opamp is in micro-volts according to datasheet. I have tried removing the capacitor C14 shorting both 1.5K resistors, etc. with no luck.

Relay is currently non-functional is normally connecting the 10K to GND.

Not sure why I am getting this high offset. Any suggestions will be helpful.

  • Hello ,

    We'll look into this and get back to you soon.

    Best regards,
    Paul

  • Hello  ,

    Please correct me if I'm wrong, the issue happens in a real/actual setup and not in simulations, right?

    May I ask what are you trying to achieve on the 2nd op amp stage? What is the gain that you are trying to achieve and what is the purpose of R11 and C14? The reason why I've asked this is because from the looks of it, the 2nd op amp stage is configured in open loop. At DC, C14 will act as an open circuit and there will be no feedback path from the output to the -IN pin.

    Can you try shorting R11 and C14 and then measure the offset again at R6? Shorting R11 and C14 will configure the 2nd op amp at a closed loop gain of 1.15.

    If the measured offset is still high, can you try furthermore removing the relay, connect R6 to GND directly, and measure the offset again?

    Thank you.


    Best regards,
    Paul

  • Sorry I wasn't clear earlier the second op-amp is configured to maintain current which is set by R6. A resistor is connected between IEXC+ & IEXC- or you can short it using multimeter in current measuring mode and it will maintain 10uA as we have a 0.1V input across 10K resistor.

    The issue got resolved after I measured the voltage difference between op-amp GND and current setting resistor's i.e. R6's GND point. There were at different voltage potential due to a layout mistake, which got resolved after connecting the two GNDs externally via a wire. 

  • Hello ,

    Good to know that the issue has been resolved already.

    I will now close this thread, but in case you encountered some other issues, don't hesitate to reach out again to us Slight smile

    Best regards,
    Paul

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.