The table 2 (page 7) of the datasheet specifies the Short-Circuit Current:
- Isink of min. 35 mA
- but at TMIN < TA < TMAX, min. 10 mA
I am not sure what it then means by "minimum 35 mA" if the min. is 10 mA.
I would like to know the specification for a certain temperature range: 0° to 85°C, not the whole range. Can I get this information please?