We are having trouble with the supply voltages for the AD8047 op amp. According to the datasheet, the op amp is rated for +-6V operation. However, when implementing a voltage follower at +-6V supply, the IC pulled ~250mA and the IC became hot to the touch. After reducing the supply to +-3V, the current was normal, but the output of the follower was heavily distorted, from a 14Mhz ac input. Is the supply voltage of the AD8047 indeed +-6V, or does that value exceed the maximums for the IC? Help would be appreciated, Thank You