Post Go back to editing

About the AD820 spice model file

Category: Software
Product Number: AD820
Software Version: LTspice 24.0.12

Hello everyone on the forum.
When I used the standard AD820 op-amp model in LTspice (Ver 24.0.12), I got an impossible result.
I set the power supply voltage to 12V, but the output voltage far exceeded the power supply voltage.
Since I used the standard library, the model data for the AD820 is the ADI.lib file, but it seems likely that there is an error in the AD820 model data.

In the circuit shown in the figure, when V3 is changed between 0 and 10 V, the output should be around 5 V, nearly 0 V, but when I tried this, the output voltage remained stuck at an impossible voltage.

I was able to simulate the circuit I was supposed to be testing without any problems by using the model file uploaded on the AD820 page.
This was the first time I had ever done something like this.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.