Post Go back to editing

NC pin - is it DNC (Do not connect) or NIC(Not internally connected)

Thread Summary

The user inquires about Pin 5 marked as NC in the OP177 datasheet, asking if it is DNC (Do not connect) or NIC (Not internally connected). The final answer confirms that Pin 5 is not internally connected to the die inside the package, allowing it to be left unconnected if required for high voltage applications.
AI Generated Content
Category: Datasheet/Specs
Product Number: OP177

Hi 

OP177

Pin 5 is marked NC in the datasheet.

Is it DNC (Do not connect) or NIC(Not internally connected)?

Our application requires us to tie all floating metal to a known potential because of a High Voltage requirement. And of course I dont want to connect it to GND via a pull down if it will affect the function of the IC. If it is internally connected - I can leave the pin unconnected.

Regards,

Jac

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.