Post Go back to editing

How to use the disable pin of ADA4807-1

Category: Datasheet/Specs
Product Number: ADA4807-1

Hello

I use ADA4807-1. And I would like to enable this Op Amp always. So I use a 10kohm pull up resistor to connect to 3.3V, which is also the power supply of the Op Amp.

However, the Op Amp seems sink a lot of current. Then I change the resistor to 1Megohm. It seems the Op Amp works well.

I wonder why and How should I pull up this disable pin?

Thanks in advance!