Post Go back to editing

ADA4177 single supply operation

Category: Hardware
Product Number: ADA4177-1

Hi,

   I intend to use a ADA4177 as a differential amplifier to single ended amp before my ADC. Can I use a single supply of 3.3V to power the op amp.

This is for a battery monitoring application. the opamp will be between my mux and the ADC. While the inputs will stay within 3V it is possible that

due to misuse the input value can exceed 3,3V and can reach 28V. Will the ADA4177 fit this application. If you have other choices please advice.