Post Go back to editing

LTC6268 input current for TIA application.

Category: Hardware
Product Number: LTC6268

Hi,

We want to use the LTC6268 as a TIA to convert photodiode current into voltage.

Our photodiode current range is between 2 to 3 mA. However, the Input Protection section of the datasheet mentions that the input current should be less than 1 mA.

I want to know if our photodiode current range is safe for this application?

Thanks.

Adam Shiau

Parents
  • Hello ,

    As indicated on the part's data sheet, the input current should be limited to less than 1mA. Having input currents of around 2-3mA can potentially damage the part.





    Though may I ask, when you have chosen LTC6288, what are the key parameters/specifications that you have considered? Depending on those specs, maybe we can recommend another ADI part with a higher input current rating that will suite your application. 

    Thank you,

    Best regards,
    Paul

Reply
  • Hello ,

    As indicated on the part's data sheet, the input current should be limited to less than 1mA. Having input currents of around 2-3mA can potentially damage the part.





    Though may I ask, when you have chosen LTC6288, what are the key parameters/specifications that you have considered? Depending on those specs, maybe we can recommend another ADI part with a higher input current rating that will suite your application. 

    Thank you,

    Best regards,
    Paul

Children

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.