LTC6268
Recommended for New Designs
The LTC6268/LTC6269 is a single/dual 500MHz FET-input operational amplifier with extremely low input bias current and low input capacitance. It also features...
Datasheet
LTC6268 on Analog.com
Hi,
We want to use the LTC6268 as a TIA to convert photodiode current into voltage.
Our photodiode current range is between 2 to 3 mA. However, the Input Protection section of the datasheet mentions that the input current should be less than 1 mA.
I want to know if our photodiode current range is safe for this application?
Thanks.
Adam Shiau
Hello AdamShiau,
As indicated on the part's data sheet, the input current should be limited to less than 1mA. Having input currents of around 2-3mA can potentially damage the part.

Though may I ask, when you have chosen LTC6288, what are the key parameters/specifications that you have considered? Depending on those specs, maybe we can recommend another ADI part with a higher input current rating that will suite your application.
Thank you,
Best regards,
Paul
Hi Paul,
Thank you for the reply.
In our application, we are concerned with the current input range from the photodiode (0.2 to 2.5 mA) and low bias current (to ensure low DC error when there is no light). A bandwidth of several hundred MHz is sufficient, and the output range of the TIA is 0 to 4.2V.
Thank you.
AdamS
Hello AdamShiau,
Based on your application and requirements, AD8065/AD8066 looks the suitable part for you. You can check the part's data sheet for more details. Here is the link to the part's data sheet: AD8065/AD8066 (Rev. L) (analog.com)
Best regards,
Paul