Post Go back to editing

Issue with AD8039 Producing 5MHz Triangular Wave

Category: Hardware
Product Number: AD8039

Hello ADI,

I am using the AD8039 op-amp to produce a 5MHz triangular wave for generating PWM signals. In my simulations on LTspice, I achieved a 5MHz triangular wave, as shown in Figure 1. However, when I transfer the design to hardware, the output is limited to 2MHz, and the signal becomes distorted as shown in Figure 2.

I have ensured that stable supply voltages are used, and I have placed passive components close to the op-amp to minimize noise and interference. 

Can you help me figure out what might be causing this problem? Could you also review my design to check if there are  issues?

Thank you for your assistance.

  

Best Regards

Nasir

Parents
  • Hi,

    How does your hardware look like? Could you provide a photo? I guess on the scope the output of U1 can be seen. What is the waveform at the output of U2?

    Zoltan

  • Hello ,

    Yeah on the scope its output of U1 . The output of U2 is shown in yellow wave form  . The second image is hardware schematic.

    Thanks

  • Hi,

    I think the supply may not be decoupled properly. Since IC1B works as a comparator, the output is saturated to the supplies, but as you see, it is not a clean rectangular wave, therefore the integrator built using IC1A can’t output a nice triangular wave. In the simulation the supply is perfect. So the supply here probably has a considerable high frequency AC component.

    According to your schematic, all decoupling capacitors are 10uF, the 100nF capacitors are missing (they are recommended for proper high frequency decoupling). You only shared the schematic, the photo of the hardware could show possible wiring/layout problems too. The other parts can also affect the supply.

    So I recommend to use 100nF ceramic capacitors for decoupling (in addition to the 10uF ones) very close to the ICs, and to test the triangle wave generator separately to be sure that the supply is not affected by the other components (IC2 and IC3). Be sure that IC3B’s inputs are not floating, I do not see it on the schematic.

    Let me make one more note. I think it would be better not rely on the supply concerning the input of the integratror. You can use an SPDT analog switch (2:1 analog MUX) that has two clean DC analog inputs and use the output of IC1B to select between these voltages. This way you can have a nice rectangular waveform as the input of the integrator.

    Zoltan

  • Hello,

    Thank you for your reply. I tried adding a 100 nF capacitor in parallel with a 10 µF capacitor, but the result was the same. My main problem is that the frequency is limited to 2 MHz. Could you tell me whether the AD8039 is suitable for use as a comparator at 5 MHz? Thanks

    Nasir

  • Hi,

    According to your simulations, the opamp should be OK (although I think it is always better to use a comparator rather than an opamp as comparator). The frequency is determined by R2, C1 but also by the ratio of R5 and R3. You can try to play with their values to get higher frequency. Don't forget to test your circuit without the additional parts (IC2 and IC3) and be sure that you have proper layout, grounding. 

    I still think the main problem is with the supply, I would use an analog switch to get supply-independent square wave. 

    Zoltan

  • Hello.

    I just test with different combination of R2 and C1 . The output waveform is pure triangular wave at 800KHz as shown in figure but  when i goes above 1.5MHz signal is distorted . I think i am over driving .

Reply Children
  • Hi,

    How does the rectangular wave look like at 800kHz? It must be a quite nice square wave.

    Try also to increase R5, that should increase the frequency. Although the amplitude will be smaller, you can have higher frequency. Choose R2 and C1 to get the highest frequency good triagular wave, then try to change R5. 

    Zoltan

  • Hello Zoltan.

    Thanks for your suggestion . I try as you said and i am able to generate 3MHz triangular wave without distortion as shown in figure.   

    But after its stuck to 3Mhz even i increase R5 until 1M ohm no change in frequency only amplitude is changing. Can you suggest something. Thanks

    Farhan 

  • The ratio of R5/R3 matters, so you can also try to reduce R3. Keep R3+R5 between 1k and 10k, and change their ratio. This way you won't have too high or too low values. This way you can avoid the effect of parastic capacitances or overloading. 

  • So you mean the addition of both R3 and R5 has to be between 1K to 10K.? Or you means the ratio has to be 1:10?

  • I can only repeat what I've recommended: keep 1k < R3+R5 < 10k and vary their ratio to get different output frequencies. I suggest you to calculate the output frequency as a function of R2, C1, R3 and R5, then you'll understand their function and the circuit's behaviour. Alternatively, you can find an analysis in the web. You can also play with the values using LTSpice.

  • Hello Zoltan.

    Thanks for your help . With your help i am able to generate 5MHz signal . Thanks again

  • Hello Zoltan.

    I hope you are doing well. I am facing another problem with the same schematic. The input signal, a sine wave, is applied via X2 to a single-ended differential amplifier stage. The emitter is connected to feedback voltages ranging from -4V to 4V. When I set the feedback voltage to, for example, +2V or any value between 0V and +4V, the output at IC1, pin 1, is shifted compared to the input signal, as shown in Figure 2.Green waveform is input and blue is output wave form.

     

    Is this a problem with biasing or any other? Thanks in advance 

    Farhan

  • Hi,

    I guess you are speaking about the output of IC3 pin 1.

    I don't really understand, what is the feedback voltage. Do you apply it at X4? Why do you use this differential amplifier and feedback voltage, what is their role in your circuit?

    Zoltan

  • Hello.

    Sorry for the confusion earlier; you are correct, the output is at IC3, pin 1. I apply DC voltages ranging from +4V to -4V at X4 to attenuate the amplitude of the input signal. Normally, we set feedback voltages between 0V and +4V to adjust the input signal's amplitude.

    This circuit is a class D amplifier with feedback derived from the output. My load is a transducer, and since we use multiple transducers with different resonance frequencies, the output amplitude varies. The feedback loop detects the signal peak, converts it to a DC voltage, and this DC voltage is controlled by a trimmer and fed back to the input. This is my feedback loop diagram.

    Thanks.PDF

  • Hi,

    OK, I got it, you use it as an analog multiplier. If you apply positive voltage on X4, then the transistors' base-emitter junctions are reverse biased, thefore the do not work in the active mode. This analog multiplier only works properly for negative emitter voltages, when the base-emitter junctions of both transistors are forward biased.

    Zoltan