Post Go back to editing

LTC6090 HV Half bridge design

Category: Hardware
Product Number: LTC6090

Hello,

I've designed a half-bridge ''high-voltage''... kind of work, but:

1. Fairly stable but limited BW, I need 1Mhz -3db, I get about 300KHz ?

2. The op-amp has severe latch-up problems ! is it known the LTC6090 latch-up ?

3. With a supply -12V/+110V, what is the max. voltage input of the LTC6090 (common / differential) ?

4. With the frequency increase, from about 50KHz, the output offset varies a lot, not sure what will be the cause (practical or theoretical) ?

Thank you for comments and suggestions. 

Thank you

PS: 1M/2.2pF scope probes

LTC6090_011.asc

Parents Reply
  • Hello,

    4. With the frequency increase, from about 50KHz, the output offset varies a lot, not sure what will be the cause (practical or theoretical) ?

    It is sorted, I am using a resistive voltage divider, and the Vin+ current intake (which varie whit frequency ?) affects the Vdrop across the resistors, I've used, for now, much lower resistor values for the voltage divider.

    The rest still not as it should be...at least on paper...?

    Thank you

    Regards 

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.