Dear all,
I'm designing an transimpedance amplifier as follows:

Do I need to put a 50 Ohm resistor on the output pin of the operation amplifier to be able to use the SMA connector? or I can just connect it directly with the resistor?
Regards,
LTC6228
Last Time Buy
The LTC6228/LTC6229 are single/dual very fast, low noise rail-to-rail output, unity gain stable op amps. They have a gain-bandwidth product of 890MHz and...
Datasheet
LTC6228 on Analog.com
Dear all,
I'm designing an transimpedance amplifier as follows:

Do I need to put a 50 Ohm resistor on the output pin of the operation amplifier to be able to use the SMA connector? or I can just connect it directly with the resistor?
Regards,
Hi Andromeda8 ,
Good day. The 50-ohm resistor on the output pin is a way to ensure the stability of the circuit. I recommend to include it in the design. Thank you.
Regards,
Gilbeys