Hello,
I need to design a current source (100 mA, 2 V) and for that I'm reading AN90 (link). This application note is about current sources for laser diodes. I have some questions about the information provided in the datasheet that I'd like to raise. I hope this is the right place to do this.
Figure 2 in AN90 shows a basic laser current source comprising an op amp and a npn transistor which supplies the current. Also an enable/disable input is available.
This is a screenshot of figure 2:

I think that this the enable/disable signal needs to be isolated from the base of Q1 using a diode (see markup in red in the screenshot above). Otherwise a the input signal is fed to the base of Q1 when the current source is enabled (i.e. Q2 is off).
This diode is also included in figure 5.

That being said, I'd like to know what is the basic difference is between a design as in figure 2 (single op amp + pass transistor) and figure 5 (dual op amp and pass transistor)? Moreover, how important is it to use an instrumentation amplifier as A2 instead of a differential op amp?
I'm asking as I need the current source to have as little noise as possible in the frequency region of about 1 Hz - 100 kHz. I'd like to understand which design idea to follow to attain a low noise driver.
Thanks.
Dan
Edit Notes
Wording[edited by: Dan-o-tronic at 5:08 PM (GMT -4) on 29 Apr 2024]