LTC6090
Recommended for New Designs
The LTC6090/LTC6090-5 are high voltage, precision monolithic operational amplifiers. The LTC6090 is unity gain stable. The LTC6090-5 is stable in noise...
Datasheet
LTC6090 on Analog.com
LTC2057
Recommended for New Designs
The LTC2057 is a high voltage, low noise, zero-drift operational amplifier that offers precision DC performance over a wide supply range of 4.75V to 36V...
Datasheet
LTC2057 on Analog.com
Hi to all, the LTC2057HV has an excellent offset voltage and a very low offset drift. Is there an alternative available out, but with a higher supply voltlage than 60V? We want to measure very small voltage changes (less than 1mV) but a common mode voltage of 70V. The LTC6090 seems to be a good choice, but is has a quite high voltage drift. I would appreciate if someone has a hint.
Kind regards Chris
Hi ChrisWeb ,
Good day. We'll be looking into this query. Aside from the parameters you have stated, are there other critical parameters in your design such as the bandwidth and slew rate?
Regards,
Gilbeys
Hi Gilbert,
a gain bandwitdth of 100kHz would be sufficient. The slew Rate is not a big topick, since we only want to measure very small Signal changes of a few mV and a maximal frequeny of 1.5kHz (sinusoidal) .
Regards
Chris
Hi ChrisWeb ,
Good day. You may want to check ADHV4702, a 24 V to 220 V Precision Operational Amplifier with a 2 µV/°C maximum input offset voltage (VOS) drift, a bandwidth of 10 MHz, and an input common-mode voltage range of +/- 107 V. You can check the datasheet here: https://www.analog.com/media/en/technical-documentation/data-sheets/adhv4702-1.pdf. I hope this helps. Thank you.
Regards,
Gilbeys