Post Go back to editing

AD8065 SOT23 Thermal Resistance (Junction to Case)

Thread Summary

The user sought the junction-to-case thermal resistance (θJC) for the AD8065WARTZ amplifier. The final answer provided the θJC for the AD8065 in SOT23 package as 57.76 °C/W. The thread also referenced the AD8066ARMZ, which has a θJC of 58 °C/W.
AI Generated Content
Category: Datasheet/Specs
Product Number: AD8065

Looking for clarification on the package thermal resistance for AD8065 amplifiers. I am specifically interested in the AD8065WARTZ junction-to-case resistance, but any similar information would be helpful such as the junction-to-ambient.

The datasheet (https://www.analog.com/media/en/technical-documentation/data-sheets/AD8065_8066.pdf) lists power derating values, which are plotted in figure 3 (page 9, ABSOLUTE MAXIMUM RATINGS). These are labeled as the junction-to-ambient resistance for the three packages. 

"Figure 3 shows the maximum safe power dissipation in the package vs. the ambient temperature for the SOIC (125°C/W), SOT-23 (180°C/W), and MSOP (150°C/W) packages on a JEDEC standard 4-layer board. θJA values are approximations."

Then on page 22 (THERMAL CONSIDERATIONS), another thermal resistance value is used. 

"...especially in the small SOT-23-5 (thermal resistance of 160°C/W)."

I saw that the thermal resistance (θJC) of AD8066ARMZ is 58 °C/W, so I was hoping that the AD8065 parts had this data available too. 

 (Missing Forum Reply)  

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.