| SLA Status | Assignee | Support Status |
|---|---|---|
| SLA Closed. | Fdelaram |
Open |
AD8065
Production
The AD8065/AD80661 FastFETâ„¢ amplifiers are voltage feedback amplifiers with FET inputs offering high performance and ease of use. The AD8065 is a single...
Datasheet
AD8065 on Analog.com
Looking for clarification on the package thermal resistance for AD8065 amplifiers. I am specifically interested in the AD8065WARTZ junction-to-case resistance, but any similar information would be helpful such as the junction-to-ambient.
The datasheet (https://www.analog.com/media/en/technical-documentation/data-sheets/AD8065_8066.pdf) lists power derating values, which are plotted in figure 3 (page 9, ABSOLUTE MAXIMUM RATINGS). These are labeled as the junction-to-ambient resistance for the three packages.
"Figure 3 shows the maximum safe power dissipation in the package vs. the ambient temperature for the SOIC (125°C/W), SOT-23 (180°C/W), and MSOP (150°C/W) packages on a JEDEC standard 4-layer board. θJA values are approximations."
Then on page 22 (THERMAL CONSIDERATIONS), another thermal resistance value is used.
"...especially in the small SOT-23-5 (thermal resistance of 160°C/W)."
I saw that the thermal resistance (θJC) of AD8066ARMZ is 58 °C/W, so I was hoping that the AD8065 parts had this data available too.
(Missing Forum Reply)
crdufour - Moved from Operational Amplifiers to Amplifiers. Post date updated from Thursday, March 21, 2024 3:19 PM UTC to Thursday, March 21, 2024 3:19 PM UTC to reflect the move.
Hi crdufour ,
The thermal resistance for junction to case (θJC) of AD8065 SOT23 package is 57.76 °C/W.
Hope this information helps.
Thanks,
Mae
Hi crdufour ,
The thermal resistance for junction to case (θJC) of AD8065 SOT23 package is 57.76 °C/W.
Hope this information helps.
Thanks,
Mae