Hi, we have the following circuit, with a reference voltage of 2.22 V we are using the ADA4807-1 as a differential amplifier to feed a ADC from 0.35 to 3.3 V. The amplifier non inverting input goes from 2.5 to 4.2 V and is really slow (nothing RF), the problem as you an see in the graph where the theory values and the measured ones are shown, when the common mode is lower than 2.65 V, the gain increase or an offset appear. Any guess about what could be happening?
thanks in advance!
Umberto.
Circuit:
Output vs Common mode input: