Post Go back to editing

using LTC6268 as a TIA, but has a sinusoidal waveform which is 300Mhz in the output port

Category: Hardware
Product Number: LTC6268

Dear Sir,

   Using LTC6268 as a transimpedance amplifier (photodiode mode), with V+ as the 5V power supply, V- as GND, the non-inverting input connected to a 1.25V reference source, and the inverting input connected to the positive terminal of the photodiode. Rf is 9.09MΩ. Currently, a sinusoidal waveform of around 300MHz with an amplitude of 100mVpp is measured at the output. Below is the schematic and oscilloscope waveform measurements.so could you help for analysing why this happened?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.