Post Go back to editing

ADS simulates the op amp with an error

Category: Software
Product Number: MAX40111
Software Version: ADS2017

When ADS used the operational amplifier MAX40111, it kept reporting errors when connecting the circuit according to the example in LTSPICE. It was not clear whether the pin was wrong or what happened. The pin was set according to the data manual, which provided two kinds of pin Settings for the pipe, one is MAX40111. The other is MAX40110. I tried both, and it didn't work. Help me,please!

Thread Notes