Post Go back to editing

Reg - AD8051 Op-amp Offset Voltage

Category: Hardware
Product Number: AD8051

Hi,

I need a clarification regarding the Rail to Rail amplifier AD8051.

We have used the amplifier AD8051 in our design & we have connected the amplifier as shown in the below image.

We are receiving 200mV output offset voltage without connecting any inputs & after connecting the input terminals with ground too, what may be reason for that output offset voltage(200mV)?

Parents Reply
  • 1. We have short the input terminal(+IN) with ground.

    2. We have tested the device with the known linear input -2.4V applied in the non inverting terminal, then we have got the output as -2.55V

    3. We are measuring the output of the op-amp using digital multi meter(6th pin of the device with respect to ground).

Children
  • Hi Gokulram,

    I don't see anything wrong with the methods and configuration of your circuit that will result to such offset.
    Are you using an evaluation board or are you using a customized pcb of your own? If customized can you share the layout file?
    How many units are you observing with this behavior?

    -Goz

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.