Hello.
When using AD9665 with dual power supplies, is it possible to input a negative voltage?
The absolute maximum ratings clearly specify GND to VDD.
Best Rigars
AD8665
Production
The AD866x family are single supply, rail-to-rail output amplifiers with low noise performance featuring an extended operating range with supply voltages...
Datasheet
AD8665 on Analog.com
AD9665
Production
The AD9665 is a laser diode driver for high performance CD-RW and DVD recordable drives. It includes four channels for four different optical power levels...
Datasheet
AD9665 on Analog.com
Hello.
When using AD9665 with dual power supplies, is it possible to input a negative voltage?
The absolute maximum ratings clearly specify GND to VDD.
Best Rigars
Hi Osamu,
In the Typical performance characteristic section, it can be seen that the figure 40 is tested with an input negative voltage if the AD8665 have dual power supplies. I would recommend to not operate near the negative supply.

Also, the specification table has a condition of single supply only.
I hope this clarifies your question.
Thanks,
Mae
Thank you.
I think the top rule is the absolute maximum rating.
So, I checked the input voltage range in the previous question.
I was convinced.