Hi,
I'm trying to get the MAX40089 spice model to work in LT Spice. I don't really need a dual opamp (the model is configured that way), but I need the de-compensated version of the MAX40079 which is the MAX40087 or MAX40089. I downloaded the model from the Analog Devices MAX40089 web page.
I made a symbol for4578.MAX40089 Test Circuit -001.asc a dual opamp matched to the (non-standard) pin list in the MAX40089 spice model.
I get the following error
Fatal Error: Unknown subcircuit called in:
x:u1:_1 out«:outa» v-«:vss» n002«:ipa» n001«:ina» u1:vdd1 u1:opamp
Thank you,
Morty