Hi
I have a problem ltc6254 is drawing 10X the current in operation mode 30mA instead of 3mA...
I need to test it for driving A/D
R= 4.7K
the cap is mostly unassembled except for the power
Thanks!
LTC6254
Last Time Buy
The LTC6252/LTC6253/LTC6254 are single/dual/quad low power, high speed unity gain stable rail-to-rail input/output operational amplifiers. On only 3.5mA...
Datasheet
LTC6254 on Analog.com
Hi
I have a problem ltc6254 is drawing 10X the current in operation mode 30mA instead of 3mA...
I need to test it for driving A/D
R= 4.7K
the cap is mostly unassembled except for the power
Thanks!
It appears you have 2x 100nF capacitor loads on the outputs. I think the LTC6252/3/4 will oscillate into such loads.
Thanks, but the capacitor on the load is not on the board...