Post Go back to editing

AD8675 Op-amps not following input at low voltages.

Category: Hardware
Product Number: AD8675

In my Circuit, Texas Instruments 8-channel Digital to Analog converter (DAC53608RTET) is connected to 8 x AD8675 op-amps in non-inverting mode. Output of DAC varies between 0 - 4.4VDC. I need this to be 0 - 12VDC. so I use 8 AD8675 Opamps, one for each DAC channel. Each Op-Amp has a Gain of 2.6. (Ri = 9.9K & Rf = 16.6K).

If input voltage lower than 2VDC. output does not follow input for all 8. Loading output of Op-Amp down using 4.7K resistor across the output improves behavior but still not linear..

Schematic and collected data for input voltage against DAC.

Requesting advice on how to make the output linear across the entire range. I can send out Schematic as a PDF and data collected as an Excel file. Please let me know where to send these as I cannot find a means to attach files here.

Graph below shows Output of OP-Amp using Input as shown below. Output is Non linear and varies with each op-amp below 5.2 volts.

Graph Below shows output of Op Amps improves when loaded with a 4.7K resistor but still not linear below 5.2V output

Graph Below shows Input voltage are exactly the same for All 8 op Amps.

Schematic of the entire circuit:

Edit Notes

attached a PDF Schematic file and excel data sheet.
[edited by: Saif67 at 8:14 PM (GMT -5) on 28 Jan 2024]

Thread Notes

Parents Reply Children
No Data