Hi, I'm new here. I just wanted to know if the AD848JNZ can be used to substitute an BB OPA604AP? If yes, thank you. If not, which high speed AD op-amp would be superior to the BB op-amp for audio? Thank you
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
AD848
Production
The AD848 and AD849 are high speed, low power monolithic operational amplifiers. The AD848 is internally compensated so that it is stable for closed loop...
Datasheet
AD848 on Analog.com
ADA4610-1
Recommended for New Designs
The ADA4610-1/ADA4610-2/ADA4610-4 are precision junction field effect transistor (JFET) amplifiers that feature low input noise voltage, current noise...
Datasheet
ADA4610-1 on Analog.com
Hi, I'm new here. I just wanted to know if the AD848JNZ can be used to substitute an BB OPA604AP? If yes, thank you. If not, which high speed AD op-amp would be superior to the BB op-amp for audio? Thank you
Sonusancti - Moved from Operational Amplifiers to Amplifiers. Post date updated from Sunday, January 14, 2024 6:36 AM UTC to Sunday, January 14, 2024 6:36 AM UTC to reflect the move.
Hi Sonusancti ,
The AD848 would seem an overkill for an audio application and as a replacement for the OPA604. I would recommend looking at the ADA4610-1 --- it is close to the performance of the OPA604. Let me know your thoughts regarding my recommendation, I may be able to recommend some more parts if you could share your requirements for your audio op-amp.
Thanks,
Gio
Hi Gio,
Thanks for your response. I like to learn from experimentation. But you're right, from the slew rate alone it's overkill. I'll update you.
Best regards,
Bobby
Hi,
I'm temporarily closing this thread. In case there will be additional questions, feel free to reply to this thread or post a new question. Thank you!
Regards,
Mae