Post Go back to editing

PID controller application for the AD8616

Category: Hardware
Product Number: ad8616

Hi, ADI expert

I am now preparing to use the ad8616 in a PID control application, the design simulation is as follows, the output VF3 is almost 0, I think if the positive phase (thermistor feedback voltage, Rth voltage) and reverse phase (reference voltage) of U2 are 1.5V, through PID adjustment, my understanding: its output should also be 1.5V, I don't know if this is the case, I mainly want to ask if there is a problem with the PID control circuit with the op amp, I hope to solve the doute, thank you!

       

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.