Post Go back to editing

PSpice Simulation, AD8099 stuck in saturation with single supply

Category: Software
Product Number: AD8099
Software Version: OrCAD Capture 17.4

AD8099 data sheet shows that AD8099 works with either +5/-5V supply or +5V single supply. When I'm doing simulation in PSpice, the Op-Amp works perfectly as expected in dual supply, but stuck in saturation when single +5V supply is applied, even though the output voltage should remain in the voltage swing range.

The only difference is that supply at VEE pin is replaced with -5V. Is this a simulation error or is it out of AD8099's capabilities?

Thanks for your time regarding my question.

Thread Notes