Post Go back to editing

AD8638 power supply range

Category: Datasheet/Specs
Product Number: AD8638

数据表中AD8638的供电电压范围是 5V to 16V single-supply or ±2.5V to ±8V dual-supply,那我可以V+用9V供电,V-用-5V供电吗?

The supply voltage range of the AD8638 in the data table is 5V to 16V single-supply or ±2.5V to ±8V dual-supply, then can I supply V+ with 9V and V- with -5V?

  • ADI North America will be on winter shutdown starting December 25, 2023; perhaps another community member can assist you until our return on January 8, 2024.
  • Hello , 

    Yes, you can supply it with V+ = 9V and V- = -5 V. The op amp does not have a ground terminal which means it can only see the difference between V+ and V-. Having V+ = 9V and V- = -5 V would mean that you will have a total supply voltage of V+ minus V- which is equal to 14V, and since this voltage is within the total supply voltage range of 5V to 16V, the op amp should work fine.

    Please do note that since you are using asymmetrical power supplies, you will have to pay extra careful with regards to the input voltage range and output voltage range of the part. The input voltage range / output voltage range head room and foot room to the rails should be followed to make sure that the part will operate well.

    Best regards,
    Paul

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.