Category: Hardware
Product Number: LTC2055H
I am using Opamp LTC2055H powered with +5V & -4V rails in Voltage follower configuration.
-
- In normal operation Precision Sensing, the input respects the common mode input range
- But in fault condition, the input to opamp becomes +6V or -6V (current-limited to 6uA)
- Query - Is there any detrimental effect on the Opamp’s Normal Operation performance if the above-mentioned fault condition occurs frequently ? This is critical since the normal operation application is Precision Sensing application.