ADA4895-2
Recommended for New Designs
The ADA4895-2 is a dual, high speed voltage feedback amplifier that is gain ≥ 10 stable with low input noise, rail-to-rail output, and quiescent current...
Datasheet
ADA4895-2 on Analog.com
ADA4895-1
Recommended for New Designs
The ADA4895-1 is a single, high speed voltage feedback amplifier that is gain ≥ 10 stable with low input noise, rail-to-rail output, and quiescent current...
Datasheet
ADA4895-1 on Analog.com
Hello,
I need to design a transimpedance amplifier. The bandwidth of the amplifier shall be about 500Hz and the Vr=0( photovoltaic mode). I noticed that the "photodiode circuit design wizard" does not allow to have such low shunt resistors ( it goes down to 100k). Given these operative conditions, can you tell me which are the main specs of the opamp that I need to consider? Can you recommend some part numbers?
Hi Topspin ,
Good day. Could you tell us which photodiode generic you're using for the application? Also, what was the application's expected peak current and output peak voltage?
Regards,
Gilbeys
Hi Topspin,
Good day. How about the photodiode generic you're using for the application so that we can also check the datasheet? In parallel, you may want to check this KWIK circuit for reference: 1MHz, Single Supply, Photodiode Transimpedance Amplifier (TIA) Design
Hope this helps.
Regards,
Gilbeys