Post Go back to editing

ADA4700-1 Single Supply

Category: Hardware
Product Number: ADA4700-1

Dear Experts!

Can I use ADA4700-1 with an unbalanced supply: +55V/GND? If yes, what should I take care of with this opamp?

I basically have a DC input voltage from 0 to 5V and I want to amplify it up to 45 to 55V, no AC signal is expected.

Thanks and regards,

Andras Magyar

Parents
  • Hi  ,

     Yes, you can use the ADA4700-1 with an unbalanced supply, but you should consider the input and output headroom. Based on the specification table, the input headroom must be around 3V away from the supply and the output should be 1.5 away from the supply.  

    Hope this information helps.

    Thanks,

    Mae

  • Dear Mae,

    Thanks a lot for the quick response!

    Unfortunately, our input signal is from 0 to 5V to be amplifier to 45 to 55V.

    Do you have another amplifier that is also high voltage and can do rail to rail with unbalanced supply?

    Regards,

    Andras

  • Hi Andras,

    Upon checking the Selection Table for High Voltage Op Amps ≥12V | Parametric Search | Analog Devices, it seems that we don't have an exact rail to rail amplifiers like you need. In order to have an input of 0-5V and an output of 45-55V, you may need to adjust the supply.

    For example, as seen in the parametric table, the ADA4099 is categorized as rail-to-rail input and output, but looking at the datasheet, the ADA4099 output voltage swing is typically 45mV away from the voltage rail if there's no load. 

    Hence, there's still a headroom for output in reference to supply.

    Is your system flexible with extending the supply rail?

    Thanks,

    Mae

Reply
  • Hi Andras,

    Upon checking the Selection Table for High Voltage Op Amps ≥12V | Parametric Search | Analog Devices, it seems that we don't have an exact rail to rail amplifiers like you need. In order to have an input of 0-5V and an output of 45-55V, you may need to adjust the supply.

    For example, as seen in the parametric table, the ADA4099 is categorized as rail-to-rail input and output, but looking at the datasheet, the ADA4099 output voltage swing is typically 45mV away from the voltage rail if there's no load. 

    Hence, there's still a headroom for output in reference to supply.

    Is your system flexible with extending the supply rail?

    Thanks,

    Mae

Children