Post Go back to editing

Non-constant active filter gain with LTC 2065

Category: Hardware
Product Number: LTC2065

I designed an amplifier using an instrumentation amplifier and an operational amplifier. Here, I used a 2 Hz multifeedback high pass and 100 Hz multifeedback low pass filter, but I could not get the efficiency I expected from my filters. What I need is for the pass band between 2 Hz and 100 Hz to have a constant gain, unfortunately, I can only have the constant gain I want between 15 Hz and 30 Hz. I tried to visually express the problem I was experiencing in the third image.

I would like your solutions and suggestions on where I should focus to improve the response of the filters.








Wrong picture
[edited by: atifkocak at 9:17 PM (GMT -4) on 12 Oct 2023]