BACKGROUND:I am working with a geology professor at a local university. He wants the students to do field work. In particular he would like to use a proton precession magnetometer. He was gifted one, 50 years old , no available schematic and broken.So it is time to build.
I will send details on the sensor if someone wants them.
REQUEST: I want some recommendation of the pre amplifier for the magnetometer. The signal is in single digit micro volts in the audio range (1kHz to 4kHz more or less). Noise is in millivolt range or higher. It is power line noise and rf noise. I used the AD design wizzard and have some boards coming for a suitable band pass filter.
The EVAL-ADA4625-1 seems to be a good enough unit to examine. . I have attempted using ai AD-620 instrumentation amp. for that purpose. It may work when the BP board arrives.
IN the days of old this was done with 2n2222 discrete
Comments appreciated
Tom Schmitt