Is there a Drop-in replacement of OP470GSZ?
LT1127
Last Time Buy
The LT1126 dual and LT1127 quad are high performance, decompensated op amps that offer higher slew rate and bandwidth than the LT1124 dual and the LT1125...
Datasheet
LT1127 on Analog.com
LT1125
Production
The LT1124 dual and LT1125 quad are high performance op amps that offer higher gain, slew rate and bandwidth than the industry standard OP-27 and competing...
Datasheet
LT1125 on Analog.com
LT1058
Production
The LT®1057 is a matched JFET input dual op amp in the industry standard 8-pin configuration, featuring a combination of outstanding high speed and precision...
Datasheet
LT1058 on Analog.com
OP470
Not Recommended for New Designs
The OP470 is a high-performance monolithic quad operational amplifier with exceptionally low voltage noise, 5nV/(root)Hz at 1kHz Max, offering comparable...
Datasheet
OP470 on Analog.com
Is there a Drop-in replacement of OP470GSZ?
Hi sherry ,
Good day. There were available op-amps with similar packages and the same function as that of OP470 such as the LT1125, LT1127, and LT1058.
Can you give us some details on the critical parameters you're looking for that we could use to further narrow down the list?
Regards,
Gilbeys
Hi sherry ,
Good day. There were available op-amps with similar packages and the same function as that of OP470 such as the LT1125, LT1127, and LT1058.
Can you give us some details on the critical parameters you're looking for that we could use to further narrow down the list?
Regards,
Gilbeys