Is there a Drop-in replacement of OP470GSZ?
KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
LT1127
Obsolete
The LT1126 dual and LT1127 quad are high performance, decompensated op amps that offer higher slew rate and bandwidth than the LT1124 dual and the LT1125...
Datasheet
LT1127 on Analog.com
LT1125
Production
The LT1124 dual and LT1125 quad are high performance op amps that offer higher gain, slew rate and bandwidth than the industry standard OP-27 and competing...
Datasheet
LT1125 on Analog.com
LT1058
Production
The LT1057 is a matched JFET input dual op amp in the industry standard 8-pin configuration, featuring a combination of outstanding high speed and precision...
Datasheet
LT1058 on Analog.com
OP470
Not Recommended for New Designs
The OP470 is a high-performance monolithic quad operational amplifier with exceptionally low voltage noise, 5nV/(root)Hz at 1kHz Max, offering comparable...
Datasheet
OP470 on Analog.com
Is there a Drop-in replacement of OP470GSZ?
Hi sherry ,
Good day. There were available op-amps with similar packages and the same function as that of OP470 such as the LT1125, LT1127, and LT1058.
Can you give us some details on the critical parameters you're looking for that we could use to further narrow down the list?
Regards,
Gilbeys
Assumed answered offline. If you still need assistance, please create a new thread. Thanks!