Post Go back to editing

Using AD534 instead of AD532

Category: Hardware
Product Number: AD534

Hello,

 

Could you advise me how to use AD534 like AD532.

AD532 is in "NOT for new designe" status.

So I am considering using AD534 instead of AD532.

 

Datasheet of AD534 describe “OPERATION AS A MULTIPLIER function.

This explanation says Z2 can be used  “OPTIONAL SUMMING INPUT.

So I think if Z2 pin of AD534 is connected to the GND,AD534  works same function of AD532?

(X1-X2)(Y1-Y2)/10V  +Z2    -> (X1-X2)(Y1-Y2)/10V

 

Is it correct?

Or is there any concerns?

I hope your advice.

 

Regards,

JUNICHI NAGATA

 

Parents Reply Children