- Can i use this IC as single supply configuration with +12V ?
- What can i do for short circuit protection ?
- Another alternate with high slew rate and high output current ( >100mA )
KCC's Quizzes AQQ306 about a fish stick challenge
1. First the quote of the month: " I am so clever that sometimes I don't understand a single word of what I am saying" - Oscar Wilde
2. New quiz AQQ306 about a fish stick challenge:
Here below is a pseudo fish diagram swimming to the right.
Question
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
AD8021
Production
The AD8021 is an exceptionally high performance, high speed voltage feedback amplifier that can be used in 16-bit resolution systems. It is designed to...
Datasheet
AD8021 on Analog.com
AD811
Production
A wideband current feedback operational amplifier, the AD811 is optimized for broadcast-quality video systems. The -3 dB bandwidth of 120 MHz at a gain...
Datasheet
AD811 on Analog.com
LT6200
Production
The LT6200/LT6201 are single and dual ultralow noise, rail-to-rail input and output unity gain stable op amps that feature 0.95nV/√Hz noise voltage....
Datasheet
LT6200 on Analog.com
LT1809
Production
The LT1809/LT1810 are single/dual low distortion rail-to-rail input and output op amps with a 350V/µs slew rate. These amplifiers have a –3dB bandwidth...
Datasheet
LT1809 on Analog.com
Hi Zie
What would be your application for the part? You can use a single supply configuration using +12V, although its performance is not guaranteed by the datasheet. Can you give me your required specifications so we can narrow down the list of possible alternatives.
Best regards,
Gio
My requirement is , I need to switch the Op-Amp output with +12V amplitude and pulse period of 100ns( Variable ) with respect to input LVTTL control lines. So i planned to operate it in G=5 for LVTTL input. output will go to the field( other modules ) So short circuit protection to be provided.

Hi Zie
You can use PTC resettable fuse, just consider the maximum expected load current, and also the operating temperature.
Best regards,
Gio
Hi GioBalgemino
Yes put external re-settable fuse. One more doubt i had been trying to simulate the given circuit but im unable to get the 12V switching output. Please find the simulation out here and provide your valuable suggestions.
Hi Zie
Here's the output from my simulation with G=5. By the way, note that AD8021 is not a rail to rail output amplifier so we wouldn't be able to achieve the 12V output that you mentioned.


It looks like LT6200, LT1809, and AD811 should be applicable. For more options you can browse it thru filtering the specs that you need.

Best regards,
Gio
Hi Zie
Here's the output from my simulation with G=5. By the way, note that AD8021 is not a rail to rail output amplifier so we wouldn't be able to achieve the 12V output that you mentioned.


It looks like LT6200, LT1809, and AD811 should be applicable. For more options you can browse it thru filtering the specs that you need.

Best regards,
Gio
Hi,
I believe that the question has already been answered so I am closing this thread. Thank you!
Regards,
Paul