Using LT3511 as a flyback converter with an input of 12V and producing an output of +70V and -70V.
I am using the output from the flyback converter to power V+ & V- pins of the operational amplifier(LTC6090). I am using 4 opamps in total.
I have taken the exact same circuit given in the application notes of LT3511.
Issue: When the opamps are not connected on the board the output observed is perfect, but when I solder the opamps on the board the output voltage is zero. How should I solve this problem?
Here is an image of my schematic

Thankyou for your help in advance!