Post Go back to editing

Single Ended to Differential conversion using two OpAmps - oscillations on output

Thread Summary

The user encountered oscillations around 1-2 MHz in a single-ended to differential conversion circuit using various op amps (AD8513, ADA4898, OP4177, OP4227). The final solution involved reducing the resistance values of RB, RA, R7, and R6 to 1k ohm to improve stability. The user confirmed this resolved the issue.
AI Generated Content
Category: Hardware
Product Number: AD8512

Hello,
I am having issues with a common SE to Differential conversion circuit basing on two Op Amps as shown in simulation. The problem I have is oscillations around 1-2 MHz on output. I added a capacitor in parallel to R1 (180 pF), tried different opamps (AD8513, ADA4898, OP4177, OP4227) - frequency shifts, amplitude differs but oscillations still occur. LTSpice shows a peak of gain near 2 MHz.
Could anyone explain my why this happens? What can I do to remove it?

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.