I see that the AD867X appears to have the current available at output to support its use as a voltage follower for up to a 21.2dBu signal, into a 600 ohm load (an odd number, but that’s 12.5Vpk, aka the parts’ maximum input voltage). However, this series is only specified into 10K and 2K. I assume that there would be a distortion sacrifice into a heavier load. I am interested in seeing how much. Is there 600 ohm data available for either of these parts, and if so, can it be made available?