Hi,
I am designing an amplifier chain with the ADA4870 at the end. I use it for its wide large signal bandwidth.
I test it on a breadboard with those conditions :
Vcc : +18V ; Vee : -18V
SD : around 4V above Vee achieve by a voltage divider
ON : a push button to put it to Vee else floating
I set up the circuit like the symmetrical supplies non-inverting amplifier from the evaluation board datasheet.
As soon as I turn the amplifier on, it immediately shut down.
Where is the mistake in my circuit?